Announcement

Collapse
No announcement yet.

Need Help Ethernet IP Communications Client - Compact Logix L32E Server Do-More BRX

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Need Help Ethernet IP Communications Client - Compact Logix L32E Server Do-More BRX

    I have a small machine that I have built many time using MODBUS TCP to communicate to plant control systems for commands and status and it has worked beautifully. Now I have to build the same machine but communications with plant control system using Ethernet IP to ControlLogix/CompactLogix.
    Here are the steps I have taken:
    1. BRX PLC - BRX IP ADDRESS SET TO 192.168.100.20
    *Enable and Configure Ethernet IP Explicit Message server
    Block 1 N200-N215 Class:4 Instance:101 Attribute: 3
    Block 2 N216-N231 Class:4 Instance:102 Attribute: 3
    Block 3 N232 Class:4 Instance:103 Attribute: 3
    2.Compactlogix L32E IP address 192.168.100.10
    *Configure New Module Generic Ethernet Module
    Name:EIPPUMPMOD
    HOST IP ADDRESS 192.168.100.20
    Connection Parameters Input 101 size 16
    output 102 size 16
    config 103 size 1

    The compact logix fails to connect to the BRX PLC

    Any help would be appreciated.

    Thank You




Working...
X