Announcement

Collapse
No announcement yet.

Drum repeat on Do More

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Drum repeat on Do More

    Hi all
    I was wondering if it is possible(I'm sure it is) to repeat the Drum sequence on a Do More PLC?
    Thanks!!


  • #2
    The easiest is to place a contact of the Done bit from the drum into the bottom (RST) line going to the drum. This will cause an immediate repeat.
    thePLCguy

    Bernie

    Comment



    • #3
      Sure. Use the drum structure's .Done field as the input to the RST leg. It'll free run.

      Comment



      • #4
        I got it working Thanks!!

        Comment

        Working...
        X