Announcement

Collapse
No announcement yet.

SDT0 missing in v2.5.1?

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • SDT0 missing in v2.5.1?

    I just downloaded the latest version and was creating a new sim project to look at BRX features. The default datetime system (SDT0) structure seems to be missing. Is there an initial configuration step I may have missed?

    Click image for larger version

Name:	2019-04-14_13-25-50.jpg
Views:	107
Size:	37.8 KB
ID:	122041


  • #2
    It doesn't seem to allow directly accessing bits of the elements in SDT0-7, so no using it directly in a normally open contact (which you selected) but it will work in a relational contact (e.g.= ). V2.3 looks to be the same for this.

    Comment



    • #3
      NC and NO contacts take bits. Structure members cannot be cast (e.g. SDT0.Month:2), if that's what you are wanting to do. What you could do is MOVE the structure member to a V, then use a cast on the V.
      There are 10 kinds of people in this world, those who know binary, and those who do not.

      Comment



      • #4
        Thanks. The relational contact is what I needed.

        Comment

        Working...
        X