Announcement

Collapse
No announcement yet.

Memory structure names

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Memory structure names

    Memory structure names can't have numbers in their names, and only get sixteen characters? Really? How am I supposed to name them?


    Ryan Poethke

  • #2
    You can have heap-items with numbers in their names. You cannot have a memory block with numbers (e.g. MyBlock5) because individual elements in the blocks are addressed with an ID. So to reference the first element in MyBlock5 at index 0, you would have to say MyBlock50, which looks like index 50 on the block MyBlock, not index 0 on the block MyBlock5.

    Heap-items (think structure tag) can have numbers in them. Also, you can create UDT (User Data Types) of your own structure definition with field names that can contain numbers, although these are also limited to 16 characters. Once you have a UDT defined, you can create as many heap-items (tags) of that type or create data blocks of the UDT type as you want.

    We are definitely aware of the 16 character limitation and have plans to increase that (minimally 32).
    There are 10 kinds of people in this world, those who know binary, and those who do not.

    Comment


    • #3
      MyStructureName1.MyFieldName12345 is a legal structure and field name. That can be pretty descriptive. We agree that 16 characters needs to be changed, but well over 90% of the variables in a massive package like DmD are less than 16 characters, so I wouldn't view it as an impossible limitation.

      Comment


      • #4
        I was referring to what's in the attached screen cap. I have (27) memory blocks to name, and it's gonna get messy to spell everything out in only 16 characters.

        Click image for larger version

Name:	mem block name.png
Views:	217
Size:	164.2 KB
ID:	124555

        Thanks,
        Ryan Poethke
        Attached Files

        Comment


        • #5
          fyi spelling error in the dialog.

          Comment


          • #6
            BlockI
            BlockII
            BlockIII
            BlockIV
            BlockV
            BlockVI
            BlockVII
            BlockVIII
            BlockIX
            BlockX
            BlockXI
            BlockXII
            BlockXIII
            BlockXIV
            ...
            BlockXXVII

            Comment


            • #7
              Roman showoff!

              Comment


              • #8
                BlockA, BlockB, BlockC...BlockAA

                Comment


                • #9
                  And One, Two, Three, ..., TwentySeven maxes out at 11 characters.

                  Comment


                  • #10
                    Originally posted by BobO View Post
                    And One, Two, Three, ..., TwentySeven maxes out at 11 characters.
                    That's what I ended up doing. I was just surprised at the limitation.


                    Thanks,

                    Ryan Poethke

                    Comment


                    • #11
                      Originally posted by Ryan_Poethke View Post

                      That's what I ended up doing. I was just surprised at the limitation.


                      Thanks,

                      Ryan Poethke
                      It's a trade-off. With indexed blocks of structures, the max name can already be 16+16+16+3=51...Block6789012345[Index678790123456].Field67890123456. Increasing the size to 32 makes that 99. Ladder displays start becoming very chunky when element names get that wide.

                      We understand the need, and increasing the name size has been on the roadmap for almost as long as there has been a roadmap. It's just a fairly big can of worms, so it has been kicked down the road.

                      Comment


                      • #12
                        Originally posted by BobO View Post
                        It's just a fairly big can of worms, so it has been kicked down the road.
                        Can we trade you cans of beer for cans of worms? Seriously, we'll ship you beer, just give us more characters.

                        Also, what's your favorite kind of beer?

                        Comment

                        Working...
                        X