Announcement

Collapse
No announcement yet.

BRX Channel Failure on channel 1 warning

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • BRX Channel Failure on channel 1 warning

    Hi all! After a 12 year hiatus, I'm back. And I remembered my forum password!

    I have a BX-18ED23-D on my desk that arrived yesterday. It is minimally wired, for the purpose of developing the C-more program. I'm getting a warning from the I/O system that states "Channel Failure on channel 1" for slot 0.
    Click image for larger version

Name:	ChannelFailureWarning.PNG
Views:	176
Size:	26.9 KB
ID:	125152
    Since I have no I/O wired at this time, is this warning to be expected?


  • #2
    The analog input channel is set for 4-20ma and there is nothing wired to it. Either change it to voltage or 0-20ma or wire up a sensor.
    If you have an urgent issue, please contact AutomationDirect's Technical Support team.

    AutomationDirect.com Technical Support: 1(800) 633-0405 or (770) 844-4200 Email Tech Support

    Comment

    Working...
    X