Announcement

Collapse
No announcement yet.

BRX Stepper Axis Change Speed on the fly

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • BRX Stepper Axis Change Speed on the fly

    I have a stepper motor axis that I am moving with an AXPOSTRAP command and I would like to change the speed while it's moving after the position gets above a set value. Is this possible?

    Thanks

  • #2
    Sounds like a job for AXSCRIPT
    I 'm not 100% sure AXPOSTRAP can't do that, but I really don't think it can.

    Comment


    • #3
      Originally posted by skeller2020 View Post
      I have a stepper motor axis that I am moving with an AXPOSTRAP command and I would like to change the speed while it's moving after the position gets above a set value. Is this possible?

      Thanks
      As was already said, that's what AXSCRIPT is for.

      Comment

      Working...
      X