Announcement

Collapse
No announcement yet.

P2K data view issue

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • P2K data view issue

    I just started using version 3.2.2 (4) and 'there's an issue in the data view. When expanding/shrinking an array (+/- icon), the Modbus address column comes back. I have to manually disable it every time. Anybody has the same issue?
    Thanks!


  • #2
    I looked at 3.1.1.1.
    I had the opposite experience from you. I would have to keep adding the Modbus Address column back. Hmmm. win some/lose some

    Comment



    • #3
      I have dual installation (didn't replace the old one). I checked my previous version 3.0.2.2 (1) and it has the same issue as the latest one (3.2.2 (4) ), and it didn't have it before. It looks like a shared dll is having issues.
      I'll uninstall the old one and reinstall the latest one to test.
      kewakl, do you have more than one instance installed?

      Comment



      • #4
        Originally posted by juance View Post
        I have dual installation (didn't replace the old one). I checked my previous version 3.0.2.2 (1) and it has the same issue as the latest one (3.2.2 (4) ), and it didn't have it before. It looks like a shared dll is having issues.
        I'll uninstall the old one and reinstall the latest one to test.
        Since the PAC software runs in a java sandbox, I am unsure how the .dll thing works.
        Some oddities could arise if versions share registry entries (HKCU\Software\JavaSoft\Prefs) but interpret the values differently.

        Originally posted by juance View Post
        kewakl, do you have more than one instance installed?
        YES! You would be surprised. I like to evaluate the issues that I find - from rev to old rev.
        1.4.1.1
        1.7.1.1
        1.9.2.0
        1.10.0.11
        1.10.1.1
        2.0.3.1
        2.4.4.1
        3.0.0.31
        3.0.1.1
        3.0.2.2
        3.1.0.11
        3.1.1.1

        and about to look into the 3.2.x.x series.

        Comment



        • #5
          Tested this in 3.2.2.4 and it appears to be with any column you hide when an array is expanded when collapsed and expanded again the hidden column is again visible.

          I will enter a trouble ticket with our software team.
          If you have an urgent issue, please contact AutomationDirect's Technical Support team.

          AutomationDirect.com Technical Support: 1(800) 633-0405 or (770) 844-4200 Email Tech Support

          Comment



          • #6
            Weird thing here is that it wasn't happening in my previous version 3.0.2.2
            Again, hope it gets fixed ASAP!!! It is very annoying.

            Comment



            • #7
              At home now...
              I see the unwanted columns in 3.0.2.2 and 3.1.1.1 - now I must recheck 3.1.1.1 at the shop (wrt post #2)
              I do not see either issue in 3.2.0.12, 3.2.1.1 OR 3.2.2.4
              I just installed them in that order. Tried twice. Open SW, open project, test, close/reopen project, then go to next rev. Could not duplicate either missing or unwanted columns.


              [work PC]As it applies to OP's issue, ignore all the text above! I was looking at the TagDatabase, not DataView.
              However, there is a similar issue with the tag database headers - I turn OFF ModStart and ModEnd, they come back when an array is toggled close/open.
              So, maybe fix that too. (well, this issue is present in 3.1.1.1, not present in 3.2.0.12, 3.2.1.1, 3.2.2.4)


              In a DATAVIEW
              In 3.0.2.2, 3.1.1.1 have to turn ON Modbus Address everytime that I toggle an array close/open
              --------------installed 3.2.0.12, 3.2.1.1 and 3.2.2.4 - in that order
              3.2.0.12, 3.2.1.1 Modbus Address column seem to work correctly -- dataview and tagdatabase
              3.2.2.4 works correctly ONCE. One toggle of close/open, the column is correctly honoring my setting. The second close/open, the Modbus Address column is back.

              No, Wait, What??? Now 2.0.2.2, 3.1.1.1 shows the Modbus Address every time. Maybe OP is on to something (DLL Hell). One version buggering another.
              Reinstall 3.1.1.1 did not fix. guess I am now infected!
              Now 3.2.0.12 and 3.2.1.1 work correctly ONCE.

              [home PC]Odd 'coincidence' at the end of installing 3.2.2.4, I had a message that my (new) serial mouse driver failed to install correctly.
              I do not have, and never have had a serial mouse plugged into the computer. I have a logitech mx518 moooose

              [edit] update for statement made about mod address columns in tag database
              Last edited by kewakl; 05-13-2018, 10:36 AM.

              Comment



              • #8
                Rechecking at home...
                Results got too convoluted to get a statement that I had confidence in posting.
                Some versions (3.2.1.1, 3.2.2.4) - the Modbus Address column INITIAL state depends on the last selection made in whatever version that I had open
                Some - always enabled and had to add every time that I close/open the array

                Looking at ..\Prefs\com\adc\apps\pac\desktop\data2panel, Data\View\Sub\Tableprefs changes just closing/opening an array

                I don't know what all the following chatter means, but a registry entry changing because I close/open an array(once or twice) in a dataview and the dataview preferences changing because of that close/open --- seems to point to an issue.
                I am posting this simply to assist in resolving this issue.
                ver 3.2.2.4
                blue is the original state, red is the diff state (maybe not the diff values), orange is dunno, green is just interesting
                [modbus address EXPLICITLY disabled]
                5/u0009687/u0009/Tagname/u00090/u00092147483647/u000915/u000975/u0009137/u0009/Value/u00091/u00092147483647/u000915/u000975/u0009137/u0009/Edit/u00092/u00092147483647/u000915/u000975/u0009138/u0009/Comment/u00093/u00092147483647/u000915/u000975/u0009137/u0009/u0009/u00092/u00096/u00090/u0009/Tagname/u0009/Modbus /Address/u0009/Value/u0009/Edit/u0009/Comment/u00095/u00091/u0009/Tagname/u0009/Value/u0009/Edit/u0009/Comment

                [modbus address disabled but honoring my selection for the first close/open]
                5/u00090/u0009/Tagname/u00090/u00092147483647/u000915/u000975/u000975/u0009/Value/u00091/u00092147483647/u000915/u000975/u000975/u0009/Edit/u00092/u00092147483647/u000915/u000975/u000975/u0009/Comment/u00093/u00092147483647/u000915/u000975/u000975/u0009/u0009/u00091/u00095/u00091/u0009/Tagname/u0009/Value/u0009/Edit/u0009/Comment

                [Modbus address column not honoring my selection after two close/opens]
                5/u00090/u0009/Tagname/u00090/u00092147483647/u000915/u000975/u000975/u0009/Modbus /Address/u00091/u00092147483647/u000915/u000975/u000975/u0009/Value/u00092/u00092147483647/u000915/u000975/u000975/u0009/Edit/u00093/u00092147483647/u000915/u000975/u000975/u0009/Comment/u00094/u00092147483647/u000915/u000975/u000975/u0009/u0009/u00091/u00096/u00091/u0009/Tagname/u0009/Modbus /Address/u0009/Value/u0009/Edit/u0009/Comment


                [Again modbus address EXPLICITLY disabled]
                5/u0009687/u0009/Tagname/u00090/u00092147483647/u000915/u000975/u0009137/u0009/Value/u00091/u00092147483647/u000915/u000975/u0009137/u0009/Edit/u00092/u00092147483647/u000915/u000975/u0009138/u0009/Comment/u00093/u00092147483647/u000915/u000975/u0009137/u0009/u0009/u00092/u00096/u00090/u0009/Tagname/u0009/Modbus /Address/u0009/Value/u0009/Edit/u0009/Comment/u00095/u00091/u0009/Tagname/u0009/Value/u0009/Edit/u0009/Comment


                Last edited by kewakl; 05-13-2018, 10:38 AM.

                Comment



                • #9
                  Any news on fixing this problem?

                  Comment

                  Working...
                  X