Announcement

Collapse
No announcement yet.

3.2.2.4 does not load program from P2-550

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • 3.2.2.4 does not load program from P2-550

    Hello,

    I have a P2-550, which was working with the new version 3.2.2.4, and I have downloaded a program into it.


    Today I was trying to open with 3.2.2.4 to upload the program for editing, but the software popped up a window says Transfer project from CPU and stuck there, no error no further prompt, showing 0% never ended

    So I used 3.1.0.11 and it uploaded the program and saved to my hard drive. 3.1.0.11 is unable to open the project but it can upload. Then I use 3.2.2.4 work with the uploaded file, make changes online with the PLC.

    I guess there is some kind of bug with 3.2.2.4.
Working...
X