Announcement

Collapse
No announcement yet.

p2000 loss of complete project

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • p2000 loss of complete project

    I Have a customer with a P2000 system on a machine. It lost the project and the Ip address reverted to default. any ideas on the cause of this? I was able to get a copy from the OEM and download it. Seems fine for now. I have powered off and back on to see if a simple power loss would cause this, It starts back up fine. we did have bad some bad weather last night.

  • #2
    Us too!

    Customer was running fine since November 2016, and then not in June. I made a service call to find the CPU had no program. I thought it may have been voltage spikes since this machine runs exclusively off 120 VAC, it is near-ish their machine shop, and it's been very hot so voltage might have been iffy due to air conditioners and the like.
    If you've done the very best you can, worrying won't make it any better - Walt Disney

    Comment


    • #3
      P2 family is a bit floppy in the base. May be vibration and/or incoming power noise.

      Comment


      • #4
        ControlWerks & Ridgeline Mach which firmware version is running in the CPU that had this issue?

        Comment


        • #5
          Originally posted by P3K_ADC_Eng View Post
          ControlWerks & Ridgeline Mach which firmware version is running in the CPU that had this issue?
          The version that was the most current in November 2016.
          If you've done the very best you can, worrying won't make it any better - Walt Disney

          Comment


          • #6
            Originally posted by Ridgeline Mach View Post

            The version that was the most current in November 2016.
            I would suggest upgrading CPU to latest 1.2.2.77. The power cycle issue was addressed in version 1.2.2.75 (released 11/28/2017).

            https://support.automationdirect.com...ail.php?pid=64

            Comment


            • #7
              Originally posted by P3K_ADC_Eng View Post

              I would suggest upgrading CPU to latest 1.2.2.77. The power cycle issue was addressed in version 1.2.2.75 (released 11/28/2017).

              https://support.automationdirect.com...ail.php?pid=64
              I did do that prior to reloading the program. Here's hoping it's fixed.
              If you've done the very best you can, worrying won't make it any better - Walt Disney

              Comment


              • #8
                I've had this happen twice with P2K now, separate clients, geographically hundreds of miles from each other. The biggest pain in the ass was getting the IP changed so I could remotely upload a new program. I REALLY wish it would default to DHCP instead of 10.10.10.10.

                Comment


                • #9
                  Wow, pretty scary that this can happen and that some of you have seen it multiple times. Given these stories and the issues I have been having over the past couple of months I think I am ready to abandon the Productivity platform.

                  Comment


                  • #10
                    Originally posted by dd33 View Post
                    Wow, pretty scary that this can happen and that some of you have seen it multiple times. Given these stories and the issues I have been having over the past couple of months I think I am ready to abandon the Productivity platform.
                    What issues have you had?

                    Mine was with one customer on one of the two P2K's in their facility that I installed. And as I wrote, they're basically powering it from a home outlet, with what I imagine is a lot of electrical noise. My other installs have been on equipment powered by 480 V 3PH, and I had a transformer stepping that power down to 120 volts.

                    Interestingly, the engineer I was working with at this customer who had the issue formerly worked in the credit card reader industry. He told me he was having an issue with one of their readers at an IBM facility, and that issue was always at the same time of day. He discovered that they had a process in operation that placed a heavy load on their 120 V supply, effectively making enough noise to render his readers inoperative.

                    I really like the P2K, but if I would voice one complaint, it's their modules need a firmer attachment to the backplane.
                    If you've done the very best you can, worrying won't make it any better - Walt Disney

                    Comment


                    • #11
                      My issues started with the CHUNK_RX error, followed by SYSTEM_RESTART error. 3.2.3.3 stopped the CHUNK_RX error but brought me System SRAM Err.
                      This P2K runs life support systems in an aquaculture facility, loss of the entire program would be very bad. I have recently added in a BRX that does a "heartbeat" check of the P2K via modbus TCP as a safeguard.

                      Comment


                      • #12
                        Originally posted by dd33 View Post
                        My issues started with the CHUNK_RX error, followed by SYSTEM_RESTART error. 3.2.3.3 stopped the CHUNK_RX error but brought me System SRAM Err.
                        This P2K runs life support systems in an aquaculture facility, loss of the entire program would be very bad. I have recently added in a BRX that does a "heartbeat" check of the P2K via modbus TCP as a safeguard.
                        You had me at life support. Facts needs to get this figured out.
                        If you've done the very best you can, worrying won't make it any better - Walt Disney

                        Comment


                        • #13
                          Is your system on a battery backup? Have you experienced any power issues on the circuit that feeds the P2 power supply?

                          I believe both of my program loss situations were caused by brown out / black out conditions. Both times they occurred overnight during a storm.

                          Comment


                          • #14
                            We have had the same issue several times with the P2000 losing it's memory. Then no way to get the IP address reset to do a remote download. There needs to be a way to set IP from the keypad. Just had another one this morning. Not sure how I'm going to get it resolved as I am 300 miles away.

                            Comment


                            • #15
                              Program loss is scary!!!
                              @whitejw: do you have latest firmware?

                              So far I haven't had any program loss (I am using latest firmware), but I am considering abandoning P2000 since there are have been too many bugs, including one or two in instructions (which has not been fixed yet!!!!), which have caused existing systems can't operate under certain configuration... and they are far away with no communication access!!!
                              Not to mention the unreliability of the suite, when a change is made something else breaks, and the overall development is very cumbersome.

                              If blackouts caused this, then becomes out of the equation, if compared with other PLC's where they really stand these situations.
                              Will have to do a stress test with power outages to see what happens.

                              Comment

                              Working...
                              X