Announcement

Collapse
No announcement yet.

Several factors affect the HSO 2000 productivity

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Several factors affect the HSO 2000 productivity

    Several factors affect the HSO 2000 productivity

    With the output of 2000 and HSO (High-Speed Output) connection SureServo SVA-2100 that I have been working for nearly 2 weeks

    This app is explained to an indexer on a punch. Electric motors and presses are designed to chisel the stack of used rollers.

    Some photos of the product

    That is the configuration Hr card SO - SETUP / HARDWARE CONFIG ... need to limit the output to the expected speed using the hormon


  • #2
    If you need to limit the output of the HSO module then go into Hardware Config, select the base group your HSO module is in, select the HSO by double clicking on it. Then select the Channel Setup that you are using, then scroll down to the Output Limits. This is were you setup the HSO output limits. Put values or variables into Maximum Velocity, Maximum Acceleration and Maximum Deceleration. This will limit the output of your HSO module.

    Comment

    Working...
    X