Announcement

Collapse
No announcement yet.

governor

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • #31
    Looking at the instructions Do More seems to have more math including great than, less than and if. Do more has more instructions and a more complete write up than productivity. Anybody have any thoughts?
    Do more simulator is a plus also.
    Last edited by fitz; 10-04-2018, 12:34 AM.

    Comment



    • #32
      In the productivity series the >, <, = and so on is under contacts - compare contact. I do use that instruction often and it works well.

      Comment



      • #33
        In Productivity I believe you can do just about anything you could imagine in the math block except for the greater than, less than, equal to. If you want to compare one math result to a constant or another tag or another math result then you must use the compare contacts instruction and compare your math stuff there. So it can do the same thing, it just separates it out instead of running two math operations inside a single math block and then comparing them within the math block.

        Comment

        Working...
        X