Announcement

Collapse
No announcement yet.

Error occured when loading dataview---attempting to open a project

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Error occured when loading dataview---attempting to open a project

    For some reason, a new a fun issue has came up. When I attempt to open any previous project in Laptop1 I get an error. I cannot then change any of the comments, modbus addresses, etc in tagname database. I can create new tags while in ladder logic, but once created I cannot then modify in the tagname database. The same project over on another laptop works fine. This issue just seemingly arose from nowhere yesterday.

    Click image for larger version

Name:	Psuite_Fd_DataviewTagdb.png
Views:	68
Size:	210.7 KB
ID:	120074

  • #2
    Looks like a corrupt project. Looks like 3.4.0.16 had a bug fix for something corrupting a project. Have you tried the latest sw 3.4.1.1? If you create a system report from the same project on both laptops. ( The bad and the good) and send to ADC they can see what is causing the project to be corrupted.

    Comment

    Working...
    X