Announcement

Collapse
No announcement yet.

Peak Scan Times

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Peak Scan Times

    Hey All,

    What is the best way to diagnose a peak scan time? AVG Scan Interval is around 12.7ms but I have a peak interval of 220.7ms. I am getting intermittent HMI timeouts so I thought it may line up with this peak scan being hit but I have no way to find out when it happens. Any pro tips to isolate this kind of issue?


  • #2
    You could use a compare instruction to compare the Peak Scan Interval or Peak Logic Scan a set value and copy the date and time into another location to see if you can pinpoint it to certain time. For instance you could do this and see if that peak time is only when you do a runtime transfer.

    Comment

    Working...
    X