Announcement

Collapse
No announcement yet.

Data collection on P2K - recommendations?

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Data collection on P2K - recommendations?

    Started out working on only 1 PLC where I was just going to grab the log files and create something in excel to generate charts. Now it looks like I'll need to start hooking up sensors to everything in the plant for continuous data collection (1 minute intervals at most) while adding a little more automation. Any recommendations for collecting continuous data from a couple dozen PLCs? Near future is just P2k/p3k PLCs, but I might throw in some click and brx PLCs based on the application requirements/cost. If multiple PLCs writing to a database server continuously is a problem, an acceptable solution would be recording the data locally and writing it to the server once per day and in some cases, once per week.

    Thanks!

  • #2
    Its too bad Point of View software is no longer sold by Automation Direct. That was cheap(ish) and had very nice integration with AD PLCs. You could use this software instead as it is also on the cheaper end of things:
    DAQFactory
    Last edited by MikeN; 04-16-2019, 04:11 PM.

    Comment


    • #3
      I haven't used it but i know there is a dedicated instruction to dataworx in the productivity suite

      https://www.automationdirect.com/adc...c/pc-datplc-un

      Comment


      • #4
        If a BRX is in the mix, could it be a data aggregator/concentrator. You could then use DMLogger.

        Comment


        • #5
          The built in datalogging for Productivity is pretty rudimentary, probably why the OP is looking for a real solution. I have used BRX before as a datalogger, it does work quite well. I can use the file log instructions to record any memory address I want and email the log to a work email address any time I want. While it does work well, a SCADA type software with logging capabilities would still work better for such a large scale logging operation IMO. You get more visual indicators of each thing you are keeping track of and logs can be output into database or excel in an easier manner. BRX wants to log things as .CSV files, which for me anyway are more cumbersome to work with.

          Comment


          • #6
            Originally posted by MikeN View Post
            Its too bad Point of View software is no longer sold by Automation Direct. That was cheap(ish) and had very nice integration with AD PLCs. You could use this software instead as it is also on the cheaper end of things:
            DAQFactory
            As an FYI, Point of View (white label of InduSoft) is no longer sold by AD, however, InduSoft can still be purchased from other authorized re-sellers. InduSoft is exactly the same as Point of View, and I find it excellent.

            It is too bad that AD no longer sells Point of View... I must say.

            Comment


            • #7
              I would look at AdvancedHMI. This is free software written in VB.net and runs on visual studio. Drivers for Modbus TCP and RTU are included to get information out of the PLCs.
              Click to AdvancedHMI
              https://accautomation.ca/click-plc-a...communication/
              BRX to AdvancedHMI
              https://accautomation.ca/brx-plc-adv...on-modbus-tcp/
              Productivity 1000 to AdvancedHMI
              https://accautomation.ca/productivit...communication/

              Depending on the database that you are connecting would determine the way you would read and write to it using VB.net.
              https://accautomation.ca/creating-a-...n-advancedhmi/

              This is a series on using VB6 to collect data from the PLCs. It is using robust logging because it will collect the data every minute. If communication is severed, the PLC will continue to log the information in the PLC until the communication is restored. The information is then all retrieved.
              Now You Can Have Robust Data Logging for Free
              (PLC Program – Modbus TCP (VB6) – Access Database – Web Server)
              Part 1 / 2 / 3 / 4 / 5 / 6 / 7 / 8 / 9 / 10 / 11 /12

              Hope this helps you out.
              Regards,
              _________________________________________________
              Garry
              ACC Automation
              https://www.accautomation.ca
              Connect with us on Facebook: facebook.com/accautomation/

              Comment


              • #8
                Thanks, Garry... Finally getting around to installing visual studio to try this out on my laptop before fully implementing it.

                Comment


                • #9
                  Be sure you install a version of VS that Archie supports.

                  Comment


                  • #10
                    Originally posted by Garry View Post
                    I would look at AdvancedHMI. This is free software written in VB.net and runs on visual studio. Drivers for Modbus TCP and RTU are included to get information out of the PLCs.
                    Click to AdvancedHMI
                    https://accautomation.ca/click-plc-a...communication/
                    BRX to AdvancedHMI
                    https://accautomation.ca/brx-plc-adv...on-modbus-tcp/
                    Productivity 1000 to AdvancedHMI
                    https://accautomation.ca/productivit...communication/

                    Depending on the database that you are connecting would determine the way you would read and write to it using VB.net.
                    https://accautomation.ca/creating-a-...n-advancedhmi/

                    This is a series on using VB6 to collect data from the PLCs. It is using robust logging because it will collect the data every minute. If communication is severed, the PLC will continue to log the information in the PLC until the communication is restored. The information is then all retrieved.
                    Now You Can Have Robust Data Logging for Free
                    (PLC Program – Modbus TCP (VB6) – Access Database – Web Server)
                    Part 1 / 2 / 3 / 4 / 5 / 6 / 7 / 8 / 9 / 10 / 11 /12

                    Hope this helps you out.
                    Regards,
                    That is a truly fantastic tutorial. I wish those existed back before I had settled on EA9's.

                    I really wish Archie would develop a driver for PxK that aHMI to talk "natively" to PxK using tag names instead of modbus addresses. I got really, really spoiled with EA9 and not having to screw with modbus address creation.

                    Comment


                    • #11
                      There are a couple of other alternatives we are using to monitor a number of P1000s/P2000s.

                      For larger applications we run Ignition, expensive but top of the line. https://inductiveautomation.com/

                      For PLCs that support MQQT output check out Initial State. Initial state is pretty cool, it lets you create web HMIs for data collected for about $10/month.

                      DaqFactory is also an excellent tool.

                      Hope this helps.

                      Comment

                      Working...
                      X