Announcement

Collapse
No announcement yet.

MQTT Client Support

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • MQTT Client Support

    any plans on implementing MQTT Publish and Subscribe to the Productivity Series PLC?? Possible as an extension to the Tag Database. I would be very interested if it could also support the Sparkplug extension for Ignition.

  • #2
    I would also be very interested in this

    Comment


    • #3
      Another hat in to the ring as an interested party.

      Comment


      • #4
        another. 10 characters to appease the forum overlords

        Comment


        • #5
          me too....this would be quite useful

          Comment


          • #6
            Add me to the list.

            I'm working with a client right now who is really pushing me to use MQTT over Modbus, which would mean I end up with BRX (not that it's a bad thing, I'm just not anywhere near as comfortable with the software). This project is going to end up using ~1000's PLC's a year for the next 5-6 years.

            Comment


            • #7
              Bump

              AD must only have 1 developer that shares their time between multiple products. This is a rather simple thing to implement AD.

              Your development pace could use some improvments.

              Comment


              • #8
                One more in support of MQTT...

                Comment


                • #9
                  YES, this would be great.

                  Comment

                  Working...
                  X