Announcement

Collapse
No announcement yet.

Internal Booleans listed as Discrete Outputs

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Internal Booleans listed as Discrete Outputs

    C-000642 , 644 and 651 are Discrete Outputs.
    How does this work if the System ID is within the 'C' datatype address space?
    I figured out that I can change the 'Type' in the 'Type' column - Please explain how this would be useful?
    I do not remember selecting these three to be 'Discrete Outputs.'
    Click image for larger version

Name:	BoolOutputs.png
Views:	69
Size:	51.2 KB
ID:	123175


  • #2
    This option of assigning a C address to a discrete output is for tag I/o reassignment (help topic P264). If you know your tags but don't have hardware figured out yet, then you can clear out the default tags for an I/O point and then reassign on of your previously created Discrete output tags to this address and then the system ID will change to the standard DO-x.x.x.x format.
    If you have an urgent issue, please contact AutomationDirect's Technical Support team.

    AutomationDirect.com Technical Support: 1(800) 633-0405 or (770) 844-4200 Email Tech Support

    Comment



    • #3
      Wow! Glad I asked!
      Thanks

      Comment

      Working...
      X