Announcement

Collapse
No announcement yet.

Productivity Suite analog channel select UI bug

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Productivity Suite analog channel select UI bug

    Setting up a new project and I've got a couple P2-08THM modules. In the hardware configuration dialog I tried to turn off the unused channels (I think that's what the "Ch. Select" column is for, the manual isn't very clear about it). Anyways, when I click a check box on a channel it checks all the rows above while clearing all the rows below. Pretty sure this isn't the intended behavior.

    Project is for a P2000, suite v3.5.0 (16)

  • #2
    It appears that used channels must be sequential from 1. When clicking a check box ON you are saying I am using all channels from 1 to this one. The selection checks reflect that.
    thePLCguy

    Bernie

    Comment


    • #3
      Looks like it works in 3.5.0.16 like it has always worked in previous version. It does not let you skip channels so if you check a channel below channels that are not checked it will check all the ones above it. Likewise if you uncheck a channel with channels below it that are checked it will uncheck them.

      Comment

      Working...
      X