Announcement

Collapse
No announcement yet.

P1-540 unable to send email notifications with new firmware 1.2.8.25

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • P1-540 unable to send email notifications with new firmware 1.2.8.25

    I have recently received this email message:
    "I have two PLCs with model code P1-540. On one PLC I have firmware version P1-540 1.2.7.37, and I am able to send email notifications.
    On the second PLC, I have firmware version P1-540 1.2.8.25 and I am unable to send email notifications, I get the error message " Failed TLC handshake (-188) ".
    Have you seen this behavior with the newer firmware?
    Would you please send me firmware version P1-540 1.2.7.37 so that I may try downgrading the firmware on the failing PLC to check if it resolves the email notification error.
    Thank you,"

    I was able to send him the older firmware file.
    Can anyone shed some light on this problem?

    Thank you,
    Garry

  • #2
    Which email server are you using? Gmail, Yahoo, etc.

    Which software version are you using? Was it the same on both occasions or did the s/w also get upgraded?
    If you have an urgent issue, please contact AutomationDirect's Technical Support team.

    AutomationDirect.com Technical Support: 1(800) 633-0405 or (770) 844-4200 Email Tech Support

    Comment


    • #3
      He has resolved the issue by the following actions:
      - Download Firmware 1.2.7.37
      - Change the option "Verify Mail Server Certificate" to "No Verification"

      He is using Gmail. The software being used for both is 3.5.12.

      Thanks,
      Garry

      Comment

      Working...
      X