Announcement

Collapse
No announcement yet.

Newbie wiring in Omega pulse meter to P2-16ND3-1

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Newbie wiring in Omega pulse meter to P2-16ND3-1

    I've got a Omega FTB-4605 flow meter that I'm wanting to connect to a P2000 using a P2-16ND3-1 module to count gallons of water flow.

    Is this the correct wiring layout?

    Omega A-> +12VDC
    Omega B-> 2K Ohm Resistor -> PLC Module Input 1
    Omega C & PLC Common -> 0VDC


    Click image for larger version

Name:	omega_ftb_4605.png
Views:	141
Size:	110.0 KB
ID:	125565

    https://www.omega.com/en-us/sensors-...4600/p/FTB4605

    Thanks

  • #2
    You won't need the resistor. The module 'equivalent input schematic' shows a 14k pull-up.
    thePLCguy

    Bernie

    Comment

    Working...
    X