Announcement

Collapse
No announcement yet.

MSG instruction stopped working.

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • MSG instruction stopped working.

    I have an Allen Bradley controllogix PLC writing to a P1000 with a MSG instruction. It was working properly for months but now the MSG instruction has a error code 16#0001 with an extension code 16#0000_0204 and the heart beat i have programmed in isn't transferring.

    Do any of you have any ideas. I can go online with both PLCs so I don't think it is a network issue

  • #2
    My AB memory is failing. Is CLX/P1K over ethernet? if so, power cycle the P1K. I have seen the P3K seem like it gets glogged -- power cycle resolved. Stop/RUN would NOT resolve.

    Comment


    • #3
      yes it is over Ethernet and it is an explicit unconnected message.

      Comment


      • #4
        A power down reset on the P1000 did solve the problem. I have a heart beat timers set up in the Controllogix PLC and have the P1000 watching the heart beat which is how i found them not communicating. Is there anything in the P1000 I can look at if it stops communicating again to see if I can find root cause.

        Comment


        • #5
          thread
          I was never able to find a 'cause.' I never could reliably reproduce this issue - however - it has reared it head occasionally.
          The listed thread never had a response. I would like to think ( 4-1/2 years ago - I forget.) that I did talk with tech support - to no avail.

          Comment


          • #6
            It happened again this time I pulled a system report before I reset the PLC

            Comment


            • #7
              I updated the firmware per the AD tech I e-mailed for tech report last week and it faulted out over the weekend again.

              I pulled a system report and E-mailed it back with the same ticket.

              dose anyone know if i can go the other way around an have the productivity message the control logix and request the data instead of the way i have it that the control logix messages the productivity. the productivity looks easy to setup either way i am not sure how to set up a control logix to be an explicit server.

              Comment


              • #8
                I had this issue 4 times since this last post.

                From my research Allen Bradley control logix PCL makes it difficult to read tags from non Allen Bradley control logix PLC.

                https://literature.rockwellautomatio...m020_-en-p.pdf

                dose anyone have any ideas to keep the coms from locking up between the control logix and the p1000. in this protect i have 2 p1000s and the coms never lock up between those

                Comment

                Working...
                X