Announcement

Collapse
No announcement yet.

Network Read RX Bug

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Network Read RX Bug

    P1-540 1.2.8.30
    Grabbing Int 32s from remote project via Network Read RX
    At first I am forced to match all the data types to int 32 in the current project.
    I need to save the values to floats. If I do it in Network Read RX it gives me a "DataType MisMatch" error
    I then go to Tag Database and change current project variables from int-32 to float
    I transfer the project and I am now reading directly from int32 to float inside the network read.
    If I open the network read I get the data mismatch error again if I hit okay, but it is fine if I hit cancel.

    I would like the mismatch suppressed as the read can obliviously do conversions and this is a ridiculous work around.
Working...
X