Announcement

Collapse
No announcement yet.

P3k HSO Position tag instability?

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • P3k HSO Position tag instability?

    In the project I am working on I need to start assigning actions to happen at certain points in the motion of the machine. Using comparators against the position reported by the encoder via the HSI/O cards. I tossed a text field up on my C-more HMI so that I can monitor this position and know where to set these actions. There seems to be a problem though as while the number will advance as the machine moves, it flashes the current location and zero alternating. This makes the program miss locations. I took a short video clip of it.

  • #2
    My guess would be that your scaling is set up in a way that it jumps from 0 to 8 and your machine is oscillating from vibration right between those pulse points in the encoder, or you have something in your program messing with the position tag.


    What encoder are you using, and can you post a screenshot of your HSI module setup?
    And a screenshot of your ladder where you are doing the compare?
    Last edited by MikeN; 02-11-2020, 06:53 PM.

    Comment


    • #3
      I just tried this. I powered up the machine, jogged it out about a foot and disabled the servo via the enable switch I have wired to the drive. No change. still 0-12-0-12-0-12. I rechecked the tag itself and while a number of instructions are reading from it, none of them should be writing to it

      . I'm sure it will be something stupid and I'll figure it out in the morning.

      Comment


      • #4
        What version firmware are you running in both the P3-HSO & the CPU?

        If you strip down the program to just the one offending instruction does it still display the same issue?

        If yes, can you create a system report and attach so I can forward this to our QA team?

        Comment


        • #5
          So is it the position of an encoder that is oscillating, or the position of a servo axis that is oscillating?

          Comment


          • #6
            Any chance you're using the Z-input reset function? This could definitely cause the problem you're seeing by resetting your count on every turn of the encoder.

            Comment


            • #7
              Originally posted by ADC_CommTeam02 View Post
              What version firmware are you running in both the P3-HSO & the CPU?

              If you strip down the program to just the one offending instruction does it still display the same issue?

              If yes, can you create a system report and attach so I can forward this to our QA team?
              I will dig into it again today and report back.

              Comment


              • #8
                Originally posted by Frontier View Post
                Any chance you're using the Z-input reset function? This could definitely cause the problem you're seeing by resetting your count on every turn of the encoder.
                I am not. I had actually considered that so I verified yesterday.


                Comment


                • #9
                  OK. With fresh eyes and a quad-shot of espresso this morning I found the issue. I had a second HSO channel set up from a previous revision that was writing to the same tag. Deleted that channel and all is well again.

                  Comment

                  Working...
                  X