Announcement

Collapse
No announcement yet.

Default Retentive Tags

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Default Retentive Tags

    Is there a setting to make all tags retentive by default? I tend to get in a hurry creating tags and forget to mark them retentive and forget that I didn't intentionally mark them retentive. I'd prefer to have to make a tag not retentive rather than make it retentive.

  • #2
    No. I recall it's due to there not being enough memory to make every tag retentive.
    Why worry? If you've done the best you can, worrying won't make it any better

    - Walt Disney

    Comment


    • #3
      Todd Dice is correct. If you look at P040 "tag database" help topic it has the below note on the retentive memory limits:

      Click image for larger version  Name:	2020-02-24_7-13-24.png Views:	0 Size:	64.8 KB ID:	128729

      Is there a setting to make all tags retentive by default?
      No. This is due to keep a user from reaching the limit described above.
      Last edited by ADC_CommTeam02; 02-24-2020, 07:25 AM.

      Comment


      • #4
        Out of curiosity why are booleans 1 byte instead of 1 bit?

        Comment


        • #5
          As far as CPU memory a Boolean data type is stored in a byte. If writing a value to a Boolean 0 = OFF; < 0 > = ON

          Comment

          Working...
          X