Announcement

Collapse
No announcement yet.

P2000 remote IO and data statistics

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • P2000 remote IO and data statistics

    I am trying to use the data statistics function for 4 RTD values coming from a remote IO rack to get the max value and i am not getting any value in my output

  • #2
    1) Is the output tag used elsewhere in the logic?
    2) PLC in run?
    3) Instruction being scanned? ( make sure no END instruction before the rung on which the instruction is placed.)
    4) Is the rung the instruction is on enabled.
    5) You can move the rung that has the instruction to the top of you logic with no logic in front of it so it is enabled all the time and place an END on the next rung to test and make sure it is not other logic. ( If possible)

    Include a screenshot of logic or the project for more assistance.

    Comment


    • #3
      Originally posted by techme View Post
      1) Is the output tag used elsewhere in the logic?
      2) PLC in run?
      3) Instruction being scanned? ( make sure no END instruction before the rung on which the instruction is placed.)
      4) Is the rung the instruction is on enabled.
      5) You can move the rung that has the instruction to the top of you logic with no logic in front of it so it is enabled all the time and place an END on the next rung to test and make sure it is not other logic. ( If possible)

      Include a screenshot of logic or the project for more assistance.
      All of what techme said and

      3.a) if the DATA instruction is in a called task, is the task being called. --experience!

      Comment


      • #4
        program example
        Attached Files

        Comment


        • #5
          thanks for the help i had an end in logic

          Comment


          • #6
            Thanks for the resolution.

            Comment


            • #7
              I see that happen quite often, it is an easy mistake to make. Wondering out loud if it is possible to have the P suite give the user a warning if you try to put code after an end instruction.

              Comment


              • #8
                WHAT! an END where it should not be? Never.

                Comment


                • #9
                  Originally posted by z28z34man View Post
                  I see that happen quite often, it is an easy mistake to make. Wondering out loud if it is possible to have the P suite give the user a warning if you try to put code after an end instruction.

                  Kind of like the program check rules in domore.

                  [edit] add quote because out of sequence post/add 'program check' wording
                  Last edited by kewakl; 02-26-2020, 02:33 PM.

                  Comment


                  • #10
                    I second the warning message prior to uploading to controller. This has gotten me more than once.

                    Comment


                    • #11
                      This will be in the next major release of the software that is currently planned for later this year. It will display a warning & in the problem report on compile and/or project transfer.

                      Click image for larger version

Name:	warning.png
Views:	42
Size:	28.0 KB
ID:	128846

                      Click image for larger version

Name:	endstatement.png
Views:	50
Size:	29.9 KB
ID:	128845

                      Comment


                      • #12
                        Nice. Quick.
                        Too bad that I was already reading this post when I got the email notification.

                        Comment

                        Working...
                        X