Announcement

Collapse
No announcement yet.

din mounting power supply

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • din mounting power supply

    Could not think of a better Title. Using the Rhino PSB24-060-P for an example. Who's idea was it to put two release levers under the power supply? Bad idea. I wrestled trying to mount the power supply to the din rail. I had to use a screwdriver on one then push it down then use the screwdriver on the opposite one to finally get the power supply down onto the rail. I can see why they thought it was a good idea, better access from both sides. I hate it. But love the power supplies.


  • #2
    Just to add to it. I think it is cause they are made out of plastic, they give too much and do not want to give way. Maybe if they were metal, it would work better.

    Comment



    • #3
      Yeah, certainly not the easiest model to mount to DIN rail, and I've used a lot of them. I've performed the two screwdriver method you described as well. Affordable? Absolutely! Easy to mount? Ummm
      If you've done the very best you can, worrying won't make it any better - Walt Disney

      Comment



      • #4
        yea very affordable and dependable. At the price, I will put up with it. Could you imagine the price if they eliminated one of the slide locks! Be cheaper yet. lol

        Comment



        • #5
          Thank you for the posts. We appreciate your business and your feedback. I have made the Product Engineer/Manager aware of your concerns. Thanks again.
          If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

          Comment



          • #6
            Originally posted by a agnone View Post
            Could not think of a better Title. Using the Rhino PSB24-060-P for an example. Who's idea was it to put two release levers under the power supply? Bad idea. I wrestled trying to mount the power supply din rail . I had to use a screwdriver on one then push it down then use the screwdriver on the opposite one to finally get the power supply down onto the rail. I can see why they thought it was a good idea, better access from both sides. I hate it. But love the power supplies.
            Bad idea to put levers under power supply

            Comment

            Working...
            X