Announcement

Collapse
No announcement yet.

Confusing ZipLink Chart

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Confusing ZipLink Chart

    Is anyone else having problems ordering the wrong modules for Ziplink? Looking at the chart for the 08nd3 and 16nd3 looks like same module, what is the parenthesis for? I ordered the wrong modules and now going to spend twice the amount of money to wire the modules. Looks like I needed the -1 for the 16 point module. I will be calling support to make sure I order the right modules and wires.
    Attached Files


  • #2
    Also it is very confusing for maintenance to look at the modules and see all the modules are labeled with the same numbers, example, (4) 16point input cards with all ziplink labeled 0 to 7/0to7. any plans to offer consecutive number labels? We do wire wrap each wire connected with the input number, but the ziplinks are not. The labels on the ziplink are pretty much useless once the wiring is completed by who does the panel.

    Comment



    • #3
      I have it figured out.

      Comment



      • #4
        Care to expound?

        Comment

        Working...
        X