Announcement

Collapse
No announcement yet.

When is this EVER an acceptable toolbar layout?

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • When is this EVER an acceptable toolbar layout?

    Somehow, I don't think that this is the first time that Cmore software has lost its layout!

    Click image for larger version

Name:	sanity.png
Views:	122
Size:	154.9 KB
ID:	108497

  • #2
    Wow, in all my years of using C-More, I never seen this happen.

    Comment


    • #3
      I've seen that before. Don't recall whether it was C-more or Click, but it was one of the two.

      Comment


      • #4
        Try selecting Window> Reset Window Layout and see if that helps.
        If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

        Comment


        • #5
          Ooooh... That's one of the buttons I have never had the guts to try!

          I start rearranging things before I ever remember that type button, by then it's too late.

          Comment


          • #6
            Originally posted by bdehner View Post
            Try selecting Window> Reset Window Layout and see if that helps.
            Should I have to? If so, why?
            Does this software just decide that my settings were junk?

            Comment


            • #7
              Can't say what their motivation is, but as a software developer, I can attest to the fact that we like to occasionally randomize the user's world just to slap them around and show them who's boss.

              Jk.

              Comment


              • #8
                "Open the bay doors, Hal..."
                If you've done the very best you can, worrying won't make it any better - Walt Disney

                Comment


                • #9
                  Originally posted by kewakl View Post
                  Somehow, I don't think that this is the first time that Cmore software has lost its layout!
                  I thought that was just how it was supposed to look! (JK, not a C-More user)

                  Comment


                  • #10
                    And now CLICK follows suit! At least consistency seems to rule!

                    Click image for larger version  Name:	SanityScreen.png Views:	1 Size:	113.2 KB ID:	108707

                    Comment


                    • #11
                      It's ADC's considered opinion that you have too much screen real estate.

                      Comment


                      • #12
                        Originally posted by ControlsGuy View Post
                        It's ADC's considered opinion that you have too much screen real estate.
                        You have never used PAC software!

                        Comment


                        • #13
                          Originally posted by kewakl View Post
                          You have never used PAC software!
                          Well, for about 10 minutes I tried it. That's why I use Do-More now!

                          Comment


                          • #14
                            UPDATE!
                            I have this again.
                            I think that I have an idea of the cause..... Spybot Search&Destroy.
                            S&D flags HKEY_USERS\S-1-5-21-2630233790-1467966773-2326387742-1000\Software\WinSystem as Spyware-000 (Rule 9F890C8B) with an elevated threat level. Silly.
                            Click image for larger version

Name:	S-D Rule 9F890C8B.png
Views:	82
Size:	8.8 KB
ID:	130148
                            I may make a burner account on their forum to report this.

                            There is a dialog after the checking. This dialog says that several suspicious registry entries exist. Hmmm. It seems that toolbar layouts are suspicious.
                            Sometime after allowing the cleanup, I see Windows UAC dialogs requesting registry changes whenever I start CLICK or CMORE software.

                            Whatever the cause, it would be a nice change for the KOYO/WINSYSTEM software to make a sane toolbar setup if it detects that there is no setup.
                            Attached Files

                            Comment


                            • #15
                              Spybot hasnt really been good software in 10 years or more now.

                              Comment

                              Working...
                              X