Announcement

Collapse
No announcement yet.

Viewmarq

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Viewmarq

    1. Viewmarq help Ver 2.01 Topic VM035 typo.
    • If the display is configured for DHCP and no DHCP server is found, the display will use APIPA to discover it's IP Address. An IP Address assigned by APIPA will have the form 169.254.x.x with a Subnet Mask of 255.2550.0.
    2. Request to add a subset of non-alpha-numeric characters from Terminal(or similar) Font.
    Code:
    (176) ░ , (177) ▒ , (178) ▓
    
    (219) █ , (220) ▄ , (221) ▌, (222) ▐ , (223)▀
    3. Change the handling of the 'Link' combobox.
    Simply opening/closing the list should not cause the software to attempt to communicate with a ViewMarq device.
    One would think that an actual click on a lineitem should be required to initiate comms.

  • #2
    Thanks for the post. I have made the Product Engineer aware of your findings/requests and as always they are greatly appreciated.
    If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

    Comment

    Working...
    X