Announcement

Collapse
No announcement yet.

product suggestion: environmental sensors

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • product suggestion: environmental sensors

    i have been looking for a low cost set of environmental sensors... temperature and humidity, that talk modbus natively, either serial or TCP. different form factors would be a plus (one that is suitable for indoor, looks like a wall mount thermostat, a IP67 rated probe that can be mounted outdoors, etc).

    this would be similar to the banner engineering m12fth3q, or many of the bravo controls products. i have had quality and accuracy issues with the bravo controls products, but the banner's price is a bit higher than id like.

    hope you can come up with something!


  • #2
    Iíve got a temp humidity sensor called hitsan, works well on rs485 modbus. From amazon, even cheaper on eBay.

    Comment



    • #3
      Dwyer's not super expensive, and I haven't seen any issues when I've used them. Vaisala's good, though sometimes spendy.

      Comment



      • #4
        dwyer doesnt do modbus natively, viasala is expensive... the banner is cheaper...

        i tried some of the chinese ones on ebay, but there is like NO documentation on them, register map, etc...

        Comment



        • #5
          Thanks for the request. I have forwarded it to the Product Manager for consideration.
          If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

          Comment

          Working...
          X