Announcement

Collapse
No announcement yet.

Open Controller Platfrom

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Open Controller Platfrom

    • Click
      • Ability to Write your own instructions in C or C++ and import them into the Click Programming environment, so you can use them in your ladder logic.
      • A plugin API for the click programming environment (IDE) so that you can extend the functionality with custom code. preferable.Net Core / .Net Standard Based.
      • A Raw controller version of the Click CPU that lets you dump your own custom C or C++ Program into the controller in place of normal Ladder.
    • Productivity
      • IEC 61131-3 User Defined Function Blocks and Functions, with Polymorphism for the Function Blocks.
      • A plugin API for the Productivity programming environment (IDE) so that you can extend the functionality with custom code. preferable.Net Core / .Net Standard Based.
      • Ability to Write your own instructions in C or C++ and import them into the Productivity Programming environment, so you can use them in your ladder logic.
      • A Controller with a Secondary ARM CPU and components (IE Built in RaspberryPi) so that you can run Linux and High-Level Code on an OS along with the PLC program. (This would be huge for us at my company.
        • This would also Allow Codesys to run on the Second CPU if you wanted.
        • Also, a dedicated bus between the PLC CPU and the ARM CPU so that they can talk to one another without using bandwidth on other communication media.
    Last edited by theColonel26; 05-16-2019, 08:27 AM.

  • #2
    Thanks for the post. I forwarded your feedback to the appropriate Product Engineers for consideration. We are always looking to improve our PLC lines and your feedback is very important so thanks again.
    If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

    Comment

    Working...
    X