Announcement

Collapse
No announcement yet.

POM for BRX PLCs

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • POM for BRX PLCs

    How about a POM for the BRX PLC that has a USB-A port? I can see several use cases:

    1) Plug in a USB flash drive for data logging; the micro SD card slot is nice, but not as easily accessible or remote-able as a USB port. This is important so that operators don't have to open the control cabinet to pull the memory device.

    2) PLC to act as a USB device server to present a virtual USB port over the network. Something similar to this: https://www.seh-technology.com/produ...s/inu-100.html

    3) Simple printer support, so the PLC could print reports or other data without the need for a computer.


    Thanks,

    Ryan Poethke

  • #2
    Thanks for the post, I sent it along to the Product Manager for consideration.
    If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

    Comment

    Working...
    X