This thread is just to document and track this error.
CPU P3-550
FW 1.1.14.38 / SW 1.9.2.0
(2 remote bases) P3-RS FW 1.1.14.38
I also lose several other data values.
One of those values is an S32 STATION ID value that is calculated in a Run First Scan Only task.
If it is calculated on first scan, I am lost as to why it is zero.
This S32 is used to build a string to display on a CMore. The string is EMPTY when this issue shows up.
The Error History has several E01802 System SRAM Err ID_FW IntE entries. I have just recently installed a UPS for each station, so will have to remember to update this thread if the UPS resolves this issue
CPU P3-550
FW 1.1.14.38 / SW 1.9.2.0
(2 remote bases) P3-RS FW 1.1.14.38
I also lose several other data values.
One of those values is an S32 STATION ID value that is calculated in a Run First Scan Only task.
If it is calculated on first scan, I am lost as to why it is zero.
This S32 is used to build a string to display on a CMore. The string is EMPTY when this issue shows up.
The Error History has several E01802 System SRAM Err ID_FW IntE entries. I have just recently installed a UPS for each station, so will have to remember to update this thread if the UPS resolves this issue
Comment