Announcement

Collapse
No announcement yet.

SIO-MB04THMS units

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • SIO-MB04THMS units

    I was reviewing the documentation on the new Stride SIO-MB04THMS that I'm planning to add to a panel tomorrow (mine hasn't arrived yet). I'm excited that AD finally offers something with excellent input isolation for thermocouple inputs. However, I'm noticing that the units reported are Celsius, with no apparent way to get the module to convert the readings to Fahrenheit. While I can do this in the 06 PLC I will be polling it with, it would be way more convenient to have the numbers come over as F to begin with. Please consider adding that option.

  • #2
    It does appear that there are 13 unused bits in the system flags register.
    Maybe the devs could co-opt one for a C/F switch. Then someone will want Kelvin, so use two switches for Unit Select.

    Comment


    • #3
      Thanks for the suggestion, I have forwarded it to the Product Manager for consideration.
      If you have an urgent issue, please contact AutomationDirect's Technical Support team at 1(800) 633-0405 or (770) 844-4200. Thank you

      Comment

      Working...
      X