Announcement

Collapse
No announcement yet.

What is errorcode P029 on the C-More Micro 6" collar display

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • What is errorcode P029 on the C-More Micro 6" collar display

    The error code flashing is P029:H=00001,P= (it keeps changing)
    Has anyone came across the error code?


  • #2
    Connected to a Do-more? I didn't see it listed in the C-more Micro helpfile, but C-more says that's "PLC Memory Version Error". Inside the PLC something must be writing to DST24 $DefaultBlockVer. Power-cycle the PLC into Stop and see what happens, then put the PLC into Run.

    Comment


    • #3
      Plugging the HMI RS-232 communication cable into the CPU ethernet port will cause this error too.

      Comment

      Working...
      X