Announcement

Collapse
No announcement yet.

Can I get a larger font size on the 8 inch?

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • Can I get a larger font size on the 8 inch?

    Using the EA9-T8CL I want to just display a count from 0 to 99. It is for a marketing display. I want the number to fill the entire screen but the largest font I found for numeric indicator was 72. This is big, but looks small on the large screen.
    Just wondering if there is another option to make the number BIG!!
    Jeff


  • #2
    Ok sorry never mind I figured it out. Even though 72 was the largest font, I could click the A+ symbol multiple times to increase the size! DOH!

    Comment



    • #3
      You can also highlight the text size and enter a number.
      Help me to have a "DOH!" moment. What is the A+ symbol?

      Comment



      • #4
        Originally posted by mwdkmpr View Post
        You can also highlight the text size and enter a number.
        Help me to have a "DOH!" moment. What is the A+ symbol?
        I think he means the toolbar button [A^]
        Select the controls to edit and the tool button enables.

        This will allow you access to fontsizes GREATER than the edit dialog. Be sure to test, the panel may not render correctly.
        Last edited by kewakl; 02-16-2017, 09:27 AM.

        Comment



        • #5
          oh yes, sorry! It was that symbol that increases the font size. I did not know I could simply type in a number, thanks!

          Comment

          Working...
          X