Announcement

Collapse
No announcement yet.

EA3-S3ML Ethernet Error

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • EA3-S3ML Ethernet Error

    Hello,

    I am trying to use my new EA3-S3ML with my Click C0-10DRE-D. When I try to set up the panel in CMore Micro as a Click Ethernet Protocol i get an error saying: "Error GUI-182 : This Panel cannot use the ethernet protocol driver." Has anyone seen this before? I can't imaging that the ethernet port on this is only for programming via the PC and not intended to be used for PLC communication....am I crazy? I am running version 4.21 of the software and the panel has 4.21 firmware. Thanks!


  • #2
    Sounds like you have selected EA1-S3ML instead of EA3-S3ML

    Comment

    Working...
    X