Announcement

Collapse
No announcement yet.

How can a barcode ascii string be read into a EA9 and diplayed

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • How can a barcode ascii string be read into a EA9 and diplayed

    Hello All.
    Can a ASCII String be read into a EA9 and displayed ? If so what do I have to do to achieve this.
    I am able to do this with my AB Panel View Plus HMI. Not sure how to do it with the C-More
    I am using a AllenBradly CompactLogix PLC
    Thank You Greatly
    Doug C

  • #2
    what is the format of the barcode? what is the 'content' of the barcode(alpha/numeric/both)?

    Comment


    • #3
      Format is ASCII, Content is both alpha and numeric

      Comment


      • #4
        Use the "Text Entry Object" and choose "Object Style" "Style 2". There are some caveats with this entry so make sure you check out the help file. ( Help file CM423)

        Comment


        • #5
          Thank You PSeries I will try that out and see how it works.

          Comment


          • #6
            I meant to post this earlier:
            I am using a USB barcode scanner on an EA7 in (devices) USB port. Works well.
            Just need to have a way to set focus to the entry object (touch or tag in Option tab) and either embed a carriage return in the barcode or touch the object after scanning.

            Comment

            Working...
            X