Announcement

Collapse
No announcement yet.

C-More Maximum Tags Error

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • C-More Maximum Tags Error

    Is there a way around this issue? Is there a setting to specify how many tags can be imported?

    Error TAG-059 : Tag cannot be added. Maximum 30,000 numbers of tags exceeded.

    Thanks in advance.


  • #2
    Are you using all 30,000.
    Are some array elements (and maybe not used?)
    Are some of them PLC hardware tags that you do not need? I know that the PAC family has lot of tags that I do not use in a cmore.

    Comment



    • #3
      1.To some degree, I'm trying to streamline the system so some applications will utilize some and some others will not.
      2.A lot of 2d Arrays. Some are used in certain applications and others in different setups.
      3.I'm sure there are hardware tags that I don't need.

      Is there a way to export a filtered list from ProSuite?

      Comment



      • #4
        I guess I could filter them with excel before I import them into C-More. I am actually only exceeding the limit by 16 tags.

        Comment



        • #5
          Originally posted by pbw View Post
          I guess I could filter them with excel before I import them into C-More.
          That is how i do it.

          Comment



          • #6
            Thanks for your response.

            Comment

            Working...
            X