Announcement

Collapse
No announcement yet.

C-More Programming Software Bug

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts


  • C-More Programming Software Bug

    Running Windows 10

    In the Events Editor, under event/action type "tag". Some of the windows are sized in a manner which some items can't be interpreted or configured.

    See attached image:
    - Under Event -> Tag, the Bit State cannot be seen (you can guess at these, so a bit of a workaround).
    - Under Action -> Tag, it isn't possible to see the full configuration options, making this unusable.

    Click image for larger version

Name:	Capture.PNG
Views:	54
Size:	31.2 KB
ID:	119642


  • #2
    Do you have text scaling or DPI scaling turned on? Could be related to one of those and not specifically Windows 10

    Comment



    • #3
      AD software has issues supporting DPI/font scaling other than windows default settings

      see the vid posted here

      Comment



      • #4
        Originally posted by kewakl View Post
        AD software has issues supporting DPI/font scaling other than windows default settings

        see the vid posted here
        Hey kewakl,

        I think the DPI scaling was it (font setting is 100%). On a different monitor, menu appeared as it should. I'll try different resolution settings on the monitor that I originally noticed the issue and see if that helps.

        Thanks!

        Comment

        Working...
        X