Announcement

Collapse
No announcement yet.

How print screens with a external printer

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • How print screens with a external printer

    I im using a EA9-T7CL-R unit, and a want to print the screens in paper using a printer.
    But i don't know how can a do this?
    Someone can help me with that?

    Regards


  • #2
    A screen image can be exported using File, Export, Screen Image.
    Print the JPG file or modify in a graphics program.

    Comment



    • #3
      I just go to file>print. Uncheck everything but screen details. do a preview. If good, just print it out.

      Comment



      • #4
        Ok,
        The HMI is conected with a Do more cpu in ethernet network, and i need print the screen using a push buttom in the hmi, i will connect a printer to the network, but i dont know how can i do this..

        Comment



        • #5
          I believe the previous answers are saying that there is no direct connection. It seems that you will have to use a pic to process and send the exported screen shot to a printer.
          thePLCguy

          Bernie

          Comment



          • #6
            you might be able to set it up as you like via the ftp server built in to the c more. ie save screen captures to a network location. youd need some way at that location to detect a new file and then automatically print. you might be able to setup a pc via scripting to print then move the file to an archive folder, or delete.

            last scripting i messed with was AutoIT, fairly easy to use once you spend some time messing with it.
            Last edited by quaizywabbit; 01-05-2019, 01:56 PM.

            Comment

            Working...
            X