Announcement

Collapse
No announcement yet.

Ea3-t6cl using dynamic text

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Ea3-t6cl using dynamic text

    Hello I have used look up text to display messages about what a machine is doing, But I found when I have message 1 displayed for example open door it stays displayed until I write a zero to the message data base. I`m wondering can I use dynamic text so it will only display a message when the tag is true. Now I`m using copy data and send a number to the tag but don`t seem to understand how to set up a message base with dynamic text. Thanks in advance for some insight.

  • #2
    https://accautomation.ca/c-more-micro-hmi-object-text/

    The above post may help you out.
    Regards,
    Garry
    Click image for larger version

Name:	C-More Micro HMI Object Text 000-min.png
Views:	100
Size:	25.3 KB
ID:	121382
    _________________________________________________
    Garry
    ACC Automation
    https://www.accautomation.ca
    Connect with us on Facebook: facebook.com/accautomation/

    Comment


    • #3
      The recipe is a powerful way to use dynamic text. 1-999 numeric values translate into a large array of Text, discrete and numeric values. I used it as a rudimentary login and each machine a user has access to carries a 1. If you are interested I can share some of my project.

      Cheers,
      Bill

      Comment


      • #4
        That would be great. See now I`m using look up text and always have to keep up with the last message sent because it retains it so I have to constantly be mind full of writing a zero to it to clear it. So I just didn`t understand how I can have more than one message with dynamic text. An example would be great. I`d like to use dynamic text say for example if tag door 1 open display that in dynamic text. And if vessel over temp occurs display that message as well. I just didn`t see how to create a message data base for this Thank you I`m new with programming.

        Comment

        Working...
        X