Announcement

Collapse
No announcement yet.

C-More EA9 Dynamic range / label for analog meter

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • C-More EA9 Dynamic range / label for analog meter

    Hello. I have an application that uses interchangeable physical gauges. I want to replicate the gauge values using a C-More EA9 analog meter. I can interrogate the gauge and get its Unit of Measure, which I want to use as the meter's label, and I can get its upper range limit which I want to use as the display range max. Can these values be set dynamically like this, and if so how do I go about it?

    Thanks, Andrew.


  • #2
    Dynamic Ranges are something C-more has needed for a long time. They are not settable. What I have done is build different objects with the ranges I want and use visibility to show the correct object at the time it is needed.

    Comment



    • #3
      Thanks Bob. I imagine that it's the same story with labels?

      Comment

      Working...
      X