Announcement

Collapse
No announcement yet.

Screen Compatibility with Metal Cutting Coolant

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Screen Compatibility with Metal Cutting Coolant

    I would like to know if the screen is compatible with a metal cutting coolant called Chem Kut 5005. Below is the spec sheet on it. The coolant is a water based coolant. If the actual data sheet is needed Message me and I can email it.


    Substance / Mixture:

    Components/Ingredients CAS No. % Range*
    Distillates (petroleum), hydrotreated heavy naphthenic 64742-52-5 <30
    2-amino-2-methylpropanol 124-68-5 <5
    2-aminoethanol 141-43-5 <5
    2,2,2-nitrilotriethanol 102-71-6 <5
    *Specific percentages of composition are being withheld as a trade secret.
    *Proprietary CAS numbers are being withheld as a trade secret.
    Additional components, of which may or may not be present, in this mixture are not classified as hazardous to health or the
    environment and within the current knowledge of the manufacturer or supplier and current regulations, are required to be
    reported in this section.
    Occupational exposure limits, if applicable and available, are listed in Section 8 – EXPOSURE CONTROLS / PERSONAL PROTECTION.

    Metalworking Fluids – Particulates Not
    Otherwise Classified

    OSHA – TWA
    15 mg/m3 (8 hour)
    NIOSH – TWA REL (Recommended Exposure Limit)
    0.5 mg/m3 total particulate (10 hour / day; 40 hour work week)

    Mineral Oil (component) OSHA – PEL
    5 mg/m3 TWA (8 hours)
    ACGIH – TLV
    5 mg/m3 – TWA (8 hours) Inhalable fraction
    NIOSH – REL
    5 mg/m3 – TWA (10 hours) Mist
    10 mg/m3 – STEL (15 minutes) Mist

    2-aminoethanol (component) OSHA – PEL
    6 mg/m3 TWA (8 hours)
    ACGIH – TLV
    1 mg/m3 TWA (8 hours) – Inhalable fraction and vapor
    6 ppm STEL (15 minutes)
    NIOSH – REL
    15 mg/m3 TWA (10 hours)
    8 mg/m3 STEL (15 minutes)
    2,2,2-nitrilotriethanol (component) ACGIH – TLV
    5 mg/m3 – TWA (8 hours)

    9. PHYSICAL AND CHEMICAL PROPERTIES
    Appearance Golden to Amber Colored, Liquid
    Odor Mild Odor
    Odor Threshold Not Determined
    pH 9.30 – 9.60 @ 5.0% w/w in water
    Melting Point / Freezing Point <32°F (0°C)
    Initial Boiling Point and Boiling Range Not Determined
    Flash Point >200°C
    Evaporation Rate (Butyl Acetate @ 25°C = 1) <1
    Flammability (solid, gas) Not Applicable
    Upper Explosive Limit / Lower Explosive Limit Not Applicable
    Vapor Pressure (Water @ 20°C = 17.5 mmHg) Not Determined
    Vapor Density Not Determined
    Specific Gravity (20°C) 0.99 – 1.03
    Solubility Miscible
    Partition Coefficient (n-octanol / water) Not Determined
    Auto-ignition Temperature Not Determined
    Decomposition Temperature Not Determined


  • #2
    I guess I should state that I am wanting to use either the latest C-More or C-More Micro......

    Comment


    • #3
      From the C-more EA9 manual: https://cdn.automationdirect.com/sta...9userm/ch2.pdf

      Chemical Compatibility
      The C-more touch panels comprise three different materials that may be exposed to outside elements: a gasket, a screen sheet and a bezel.
      • Gasket material is silicone.
      • Screen sheets are PET.
      • Panel bezels are ABS plastic.

      It is really up to the user to determine the chemical compatibility from this information since the manufacturer cannot anticipate all possible exposures.

      In my experience, Ethanol and ABS do not get along well. ABS becomes brittle and falls apart. I am no chemist, but I see several components that have ethanol in their name.

      I recommend you contact the chemical provider and ask them about their compatibility with the three components above, Silicone, PET and ABS.

      Comment

      Working...
      X