Announcement

Collapse
No announcement yet.

C-more and Email Addresses

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • C-more and Email Addresses

    I find the Text Entry object lacking in some printable symbols that may be used for Email addresses. Both the Do-more/BRX/etc and the Productivity allow Strings to be used for a destination Email Addresses. It should be easy to change these through a C-More such as when a Plant Manager, Etc., changes but some symbols are missing.

    From Wikipedia:

    The local-part of the email address may use any of these ASCII characters:
    • uppercase and lowercase Latin letters A to Z and a to z;
    • digits 0 to 9;
    • printable characters !#$%&'*+-/=?^_`{|}~;
    • dot ., provided that it is not the first or last character unless quoted, and provided also that it does not appear consecutively unless quoted (e.g. John..Doe@example.com is not allowed but "John..Doe"@example.com is allowed);[8]
    The is more, but I think this gives the minimum. Currently we can only enter dot, underline, and dash.

    Adding all the legal symbols would be helpful
Working...
X