Announcement

Collapse
No announcement yet.

Question about Event Manager

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Question about Event Manager

    Does anyone know if events can be turned on and off by the operator using a tag?

  • #2
    Yes, events can be triggered by a tag.
    https://www.automationdirect.com/mic...ontent/136.htm

    Do you have a specific example that is not working?
    Regards,
    Garry
    _________________________________________________
    Garry
    ACC Automation
    https://www.accautomation.ca
    Connect with us on Facebook: facebook.com/accautomation/

    Comment


    • #3
      I think I should clarify. I was trying to find out if Events can be Enabled/Disabled by the Operator using a tag?

      Comment


      • #4
        You can set any particular event to be conditioned upon multiple tags. Say for example you have an event based upon a tag in your plc, simply add a second tag, internal to your hmi that must be on to trigger the event. Alternatively the enable tag could be located in the plc.

        Comment


        • #5
          Yes, when you add the event, set No. of Tags: to 2 and then select the appropriate logic needed.

          Click image for larger version

Name:	Event multiple tag logic configuration.jpg
Views:	40
Size:	86.5 KB
ID:	129323
          Attached Files

          Comment


          • #6
            Thanks Guys, Good idea! Im working on a cookie cutter application that will be sold as a package and the end user needs to have the ability to disable events depending on their specific setup.

            Thanks again

            Comment

            Working...
            X