Announcement

Collapse
No announcement yet.

Help with EA9 Recipes

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Help with EA9 Recipes

    Hey all,

    I'm new to C-more so be gentle... but I'm running into a problem with the recipe object in C-more EA9.

    I have several recipes that write to 40-60 tags at a time but all of them only work for 12 tags before stopping. According to the recipe "Writing X/X" readout it is writing to all tags in the recipe.

    Tags are ASCII Strings, 82 characters

    It's also worth noting that I'm using the simulator since I don't have the hardware (EA9-RHMI) on site yet. Is it potentially a side effect of using the simulator?

    Thanks for any help you can provide.

  • #2
    CMore simulator does not actually communicate. It is mainly to see a pseudo live layout with button actuation, screen changing etc. The numbers you see in the simulator are local to it. You should see the effect you need when loaded into the hardware. The limited changes you are seeing, even as local values, may be a limitation of the simulator.
    thePLCguy

    Bernie

    Comment


    • #3
      OK, cool. I thought it might be something like that. I'll update if I have the same issue with the actual hardware. Thanks for the input.

      Comment

      Working...
      X