Announcement

Collapse
No announcement yet.

Bitmap Question

Collapse
X
 
  • Filter
  • Time
  • Show
Clear All
new posts

  • Bitmap Question

    We have just started a new project with the following setup.
    EA9-RHMI setup for HD- 1280x720 project resolution
    View Sonic 32" HDMI monitor #VX3276-MHD

    I can not seem to get any of our user graphics to look very good at all.
    Our bitmaps are 300 dpi. I'm sure I'm doing something wrong.
    Even when I make a large push button it has ruff edges??
    Not sure it's me or the EA9-RHMI limits??

    Thanks ahead for any help on this.


  • #2
    Daakers, I recommend you contaxct Tech Support and be prepared to send them a project that has this issue and a photo of what you are seeing.

    Comment


    • #3
      In general it is better to determine the bit dimensions of the target position then use external imaging software to limit the dimensions of your (presumably larger) image. Only after that provide the modified image to the CMore development software.
      thePLCguy

      Bernie

      Comment


      • #4
        Originally posted by bcarlton View Post
        In general it is better to determine the bit dimensions of the target position then use external imaging software to limit the dimensions of your (presumably larger) image. Only after that provide the modified image to the CMore development software.
        I think that's what I have always done. These are floor plans. We use Autocad to re-draw the plans from scanned files, then we import to CorelDraw to convert to bitmaps. It has always worked good in the past event on the 15" EA9, and other HMI software but not so good here.

        Comment


        • #5
          Originally posted by bcarlton View Post
          In general it is better to determine the bit dimensions of the target position then use external imaging software to limit the dimensions of your (presumably larger) liteblue image. Only after that provide the modified image to the CMore development software.
          This is pretty awesome and I love this.
          Last edited by kelsien; 04-08-2020, 07:48 AM. Reason: spelling

          Comment

          Working...
          X