Announcement

Collapse
No announcement yet.

C-More v6.14 Siemens tags

Collapse
X
  • Filter
  • Time
  • Show
Clear All
new posts


  • C-More v6.14 Siemens tags

    I have a new EA9-T8CL HMI screen connected via Ethernet to a Siemens S7-300 PLC.

    There seems to be an issue with addressing tags with an address higher than 254. When I try I get error code GUI-024

    Example:
    MW250 works
    MW300 gets error code

    M20.1 works
    M520.1 gets error code


    The addresses exist in the PLC as part of a standard block of code that I would prefer not to change. Any way to get the software to allow the addresses?


  • #2
    The help file entry for S7-300 addressing shows the ranges allowed.
    thePLCguy

    Bernie

    Comment



    • #3
      Help files

      I haven't been able to get the help files to work on the new version of the software.

      Can you copy and paste the allowed ranges here please?

      Comment



      • #4
        Here is the addressing section for the Siemens S7-300. (But this is from 5.0, we don't have the higher level installed yet.)
        Attached Files
        thePLCguy

        Bernie

        Comment

        Working...
        X