Announcement
Collapse
No announcement yet.
Search Result
Collapse
10 results in 0.0045 seconds.
Keywords
Members
Tags
-
Replace SVM-220/230 with SVM 220, straight swap or need to reteach points and home?
I am getting a "ALE11: Encoder Position Dectector Error" alarm on my SVA-2300 controller. The two corrective actions are check wire connection...Last edited by bjwiest; 06-25-2019, 12:23 PM.
-
Which PID Controller for SERVO control?
Who can recommend a panel-mount PID controller for motion-control (as opposed to heat)?
So not the type where tuning begins with P at or...Last edited by Aplonis; 03-29-2019, 09:09 AM.
-
Torque Control with SureServo and Productivity PLC?
I am working to design a testing system that repeatedly applies a specified torque to rotate a set of components through a 160° arc. I'm working with...
-
Sureservo fault records
Sureservo parameter P4-00 to P4-04 are fault records in the drive. What I cannot seem to find is what is the data type? I am assuming it is a string as...
-
Delta Servo Parameter problem
hello every one, I have a cnc machine with a Y axis controlled by a 0.4KW ASDA servo motor. The motor shaft is connected to the ball screw via belt....
-
Servo Valve Control
I am wanting to write a program to control a setworks application on a sawmill carriage. Currently it has a tempsonic transducer it uses for position...
-
Torque
im basically creating a pan tilt head for a light and the light weighs about 329oz would a servo with the torque of 330 be sufficient or do i need something...
-
Ziplink Question
Our company is running 2 servos (SVA-2100) with the Ziplink (ZL-RTB50). We have the 50-pin cables connecting each servo respectively, grounded the z...
-
Servo Drive control via RS485
Hi all, I am working on a project involving control of servo motors. I am taking a value between 0-255 communicated via RS485. I would like each v...
-
Allen Bradley ML1200 to Servo Amp
Hi everyone, Happy new year! I was wondering if someone has a simple example for interfacing an AB micrologix with a SV-2040 servo driver. I understan...